AXIS#.JOG.V

Description

This keyword sets the jog velocity. To activate jog, see AXIS#.JOG.MOVEN and AXIS#.JOG.MOVEP.

If a jog is in progress, changing this value changes the motor velocity immediately.

Versions

Action Version Notes
Implemented 02-04-01-000  

General Information

Type Read/Write
Units

Rotary: RPM, RPS, deg/s, (custom units)/s, rad/s

Linear: counts/s, mm/s, µm/s, (custom units)/s

See Velocity Units for details.

Range Depends on units. See Velocity Range for details.
Default Value

60 RPM

Depends on units. See Velocity Units for details.

Data Type Float
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
AXIS1.JOG.V

501bh

03h

Unsigned32

Velocity

-

Read/Write

No

AXIS2.JOG.V

511bh

03h

Unsigned32

Velocity

-

Read/Write

No

EtherNet/IP

Name

ID

Hex

Data Type

Access

Units

AXIS1.JOG.V

6904

1AF8

Signed32

Read/Write

Velocity

AXIS2.JOG.V

72440

11AF

Signed32

Read/Write

Velocity

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS#.JOG.V

6904

Float

Read/Write

Velocity